FB#.RES
Description
This parameter reads the actual resolution in use for the feedback deviceA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Rotary: counts/rev Linear: counts/poles |
|
Range |
Depends on type |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
|
Copyright © 2018 Kollmorgen |
|